BODE.VFLIMIT

Description

When BODE.VFLIMIT is set to 5, the firmware monitors the drive feedback velocity VL.FB. When VL.FB goes above BODE.VFTHRESH, an internal counter records the length of time VL.FB was above BODE.VFTHRESH. If the internal counter reaches BODE.VFLIMIT, Fault F133 – Instability during Autotune will be generated.

The smaller the BODE.VFLIMIT, the quicker Fault 133 will be generated when VL.FB exceeds BODE.VFTHRESH.

Example

Set BODE.VFTHRESH to 10 RPM:

-->BODE.VFTHRESH 10

Set BODE.VFLIMIT to 0.500 seconds

-->BODE.VFLIMIT 0.5

Set BODE.MODE to 5 to enable stability detection

-->BODE.MODE 5

General Information

Type

R/W Parameter

Units

s

Range

0.001 to 60.000

Default Value

0

Data Type

Decimal

Start Version

M_01-02-10-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET
Fieldbus Address Attributes Signed?

PROFINET

2650 DWord Yes
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
651 4 Byte Signed Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

1300

No 32 bit Yes M_01-06-03-000

Related Topics

Using the Performance Servo Tuner

Using the Performance Servo Tuner: Advanced