CAP0.EDGE, CAP1.EDGE

Description

The filtered trigger source is monitored for rising edge, falling edge, or both edges. The event mode logic may ignore the precondition edge detection; however, the trigger always uses edge detection.

The precondition logic has an identical feature controlled by CAP0.PREEDGE, CAP1.PREEDGE .

Value

Description

0

Reserved

1

Rising edge

2

Falling edge

3

Both edges

General Information

Type

NV Parameter

Units

N/A

Range

1 to 3

Default Value

1

Data Type

U8

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
CAP0.EDGE

PROFINET

2027 Byte No
Sercos® III 2 Octets
CAP1.EDGE

PROFINET

2040 Byte
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
CAP0.EDGE 28 1 Byte Integer
CAP1.EDGE 41
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
CAP0.EDGE 54 No 8 bit No M_01-03-00-000
CAP1.EDGE 80

Related Topics

Using Position Capture

CAP0.PREEDGE, CAP1.PREEDGE