CAP0.STATE, CAP1.STATE

Description

When enabling the capture (CAP0.EN, CAP1.EN ), this parameter is set to 0 until the next event is captured.

0 = Not captured or Capture Disabled

1 = Captured

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos®
Parameter Fieldbus Address Attributes Signed?
CAP0.STATE

PROFINET

2037 Byte No
Sercos® III 2 Octets
CAP1.STATE PROFINET 2050 Byte
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
CAP0.STATE 38 1 Byte Integer
CAP1.STATE 51
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
CAP0.STATE 74 No 8 bit No M_01-03-00-000
CAP1.STATE 100

Related Topics

Using Position Capture