CAP0.T, CAP1.T

Description

If time capture was configured, the captured time is stored in this parameter. The reference time is the occurrence of the last MTS signal (recurring every 62.5 µs), so this is a purely drive internal time.

General Information

Type

R/O Parameter

Units

ns

Range

N/A

Default Value

N/A

Data Type

U32

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

20A0h/0

CAP0.T M_01-00-00-000

20A1h/0

CAP0.T

20A2h/0

CAP1.T

20A3h/0

CAP1.T
PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
CAP0.T

PROFINET

2038 DWord No
Sercos® III 4 Octets
CAP1.T

PROFINET

2051 DWord
Sercos® III 4 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
CAP0.T 39 4 Byte Integer
CAP1.T 52
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version

CAP0.T

76 No 32 bit No M_01-03-00-000

CAP1.T

102

Related Topics

Using Position Capture

CAP0.MODE, CAP1.MODE