CMPx.OUTMASK

Description

This keyword sets the binary output disable mask between the setpoint and the drive's output pin. Note the internal setpoint state remains valid, only the external output is blocked.

Example

The following example sets an outmask to 7 (binary 111) to block setpoint states 0, 1, and 2 from asserting the drive output pin.

-->CMP0.OUTMASK 7

General Information

Type

NV Parameter

Units

None

Range

0 to 255

Default Value

0 (Inactive)

Data Type

Integer

Start Version

M_01-13-00-000

Hardware Supported

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-IC Revision DA or higher

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
5394h /0

CMP0.OUTMASK

M_01-13-00-000
539Bh /0

CMP1.OUTMASK

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
CMP0.OUTMASK

PROFINET

2916 DWord No
Sercos® III 4 Octets
CMP1.OUTMASK

PROFINET

2923 DWord
Sercos® III 4 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
CMP0.OUTMASK 917 4 Byte Integer
CMP1.OUTMASK 924
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
CMP0.OUTMASK 1832 No 32 bit No M_01-03-00-000
CMP1.OUTMASK 1846

Related Topics

Compare Engines

CMPx.SETPOINT