CMPx.STATE

Description

Use this keyword to read the state of a Compare setpoint. The state indicates whether a compare pulse is being generated. If the state is 1, then a pulse is being generated. If the state is 0, no pulse is being generated.

When accessing this keyword through a fieldbus, the values are to be interpreted as a bitmask, with each bit corresponding to one of the Compare setpoints.

General Information

Type

R/O Parameter

Units

None

Range

0 to 7

Default Value

0 (Inactive)

Data Type

Integer

Start Version

M_01-13-00-000

Hardware Supported

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-IC Revision DA or higher

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
34C0h/2

CMP0.STATE

M_01-13-00-000
34C1h/2

CMP1.STATE

PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
CMP0.STATE

PROFINET

2919 Byte No
Sercos® III 2 Octets
CMP1.STATE

PROFINET

2926 Byte
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
CMP0.STATE 920 1 Byte Integer
CMP1.STATE 927
Modbus
Parameter Register Address Is 64 bit? Attributes Signed? Object Start Version
CMP0.STATE 1838 No 8 bit No M_01-03-00-000
CMP1.STATE 1852

Related Topics

Compare Engines

CMPx.SETPOINT