DIO9.INV to DIO11.INV

Description

This parameter changes the logic sense of the differential input/output signals. When false, a logic 1 occurs when the + signal is higher than the – signal. When true, a logic 1 occurs when the – signal is higher than the + signal.

The drive output parameters DOUTx.STATE and DOUTx.STATEU are not affected by changes in this parameter. The drive input parameters DINx.STATE will be affected.

This parameter can be set at any time. It will be ignored unless DRV.EMUEMODE is set to 10.

General Information

Type

NV Parameter

Units

NA

Range

0 to 1

Default Value

0

Data Type

U8

Start Version

M_01-05-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Parameter Object Start Version

5258h /0

DIO9.INV M_01-05-00-000

5254h /0

DIO10.INV

5256h /0

DIO11.INV
PROFINET and Sercos® III
Parameter Fieldbus Address Attributes Signed?
DIO9.INV

PROFINET

2600 Byte No
Sercos® III 2 Octets
DIO10.INV

PROFINET

2596 Byte
Sercos® III 2 Octets
DIO11.INV

PROFINET

2598 Byte
Sercos® III 2 Octets
EtherNet/IP
Parameter Instance Data Size Data Type
DIO9.INV 601 1 Byte Integer
DIO10.INV 597
DIO11.INV 599
Modbus
Parameter Register Address Is 64 bit? Attributes Signed?
DIO10.INV 1192 No 8 bit

No

DIO11.INV 1196
DIO9.INV 1200

Related Topics

DIN1.STATE TO DIN7.STATE

DOUT1.STATE AND DOUT2.STATE

DOUT1.STATEU AND DOUT2.STATEU

DRV.EMUEMODE