DRV.DBILIMIT

Description

This parameter sets the maximum amplitude of the current for dynamic braking.

Example

Setting DRV.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

General Information

Type

NV Parameter

Units

Arms

Range

0 to minimum of drive peak current (DRV.IPEAK) and motor peak current (MOTOR.IPEAK).

Default Value

Minimum of drive continuous current (DRV.ICONT) and motor continuous current (MOTOR.ICONT).

Data Type

Float

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3444h/0

M_01-00-00-000

PROFINET
Fieldbus Address Attributes Signed?

PROFINET

2114 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
115 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

228

No 32 bit No M_01-03-00-000

Related Topics

"Controlled Stop"

"CS Parameters"

DRV.DISMODE

"Dynamic Braking"