DRV.EMUEPULSEWIDTH

Description

EMU Encoder Out Pulse Width Register

Sets pulse width for CW/CCW and Step and Direction modes. This parameter does not effect the A quad B mode. To calculate emuOutPulseWidth:

(Desired pulse width -40 nsec)/520 nsec

Requirement DSFPGA-03-306
Bits Bits Description
11:0 emuOutPulseWidth Read/Write
12 bit unsigned number minimum resolution is 520 nsec.
Reset state – 0
15:12   reserved
  • Register is in counts (12 bit)
  • Register * 520ns + 40ns is the actual pulse with.
  • Register = 1 = pulse width is 560ns = 0.56us (minimum value)
  • For each register increment the pulse width is raised by 0.52us

Example

50 usecs pulse width

emuOutPulseWidth = (50 usecs – 40 nsec)/520 nsec = 96

actual pulse = 96*520 nsec + 40 nsec = 49.88 usecs.

General Information

Type

TBD

Units

us(microseconds)

Range

4.08 us to 2621.48 us

Default Value

4.08 us

Data Type

Float

Start Version

M_01-00-00-000
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
AKD-N No
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

520Dh /0

M_01-00-00-000

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2525 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
526 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed?

1050

No 32 bit No

Related Topics

DRV.EMUEMODE