DRV.EN

Description

DRV.EN issues a software enable to the drive. You can query the value of DRV.ACTIVE to check whether the drive is currently enabled or disabled.

You can also query the value of DRV.DISSOURCES to check whether the software enable bit is high (software enabled was issued by executing DRV.EN) or the software enable bit is low (software disable was issued by executing DRV.DIS). If the drive software enable bit is low and DRV.EN is executed, then drive faults are automatically cleared during the software enable process.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

Analog drive software is enabled.

All other types of drive software are disabled.

Data Type

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos®
Fieldbus Address Attributes Signed?

PROFINET

2127 Command* No
Sercos® III

*For PROFINET, write a value of 0 into the PNU to execute a command.

EtherNet/IP
Instance Data Size Data Type
128 Command None
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

254

No Command No M_01-03-00-000

Related Topics

"Clearing Faults"

"Enable/Disable"

DRV.DIS, DRV.DISSOURCES,DRV.ACTIVE