DRV.HWENABLE

Description

Status of the Hardware Enable.

0 - not enabled

1 - enabled

Notes: This parameter reflects the status of the hardware enable only, not if the status of the power stage. The status of the power stage enable is determined by DRV.ACTIVE.

General Information

Type

R/O

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Start Version

M_01-18-00-004

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC Yes
AKD SynqNet No
AKD EtherNet/IP No
AKD PROFINET No
AKD Sercos® III No
AKD-N No
AKD-C Yes

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2527 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
528 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed?

1054

No 8 bit No

Related Topics

DRV.DISSOURCES | DRV.ACTIVE