DRV.HWENMODE

Description

This parameter selects the action that the hardware enable digital input will perform.

0 = The rising edge of the hardware enable will clear the drive faults.

1 = The rising edge of the hardware enable will not clear the drive faults.

The high/low state of the hardware enable is always used to control the active enable state of the drive.

General Information

Type

R/W Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-03-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3506h/0

M_01-03-00-000

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2130 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
131 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

260

No 8 bit No M_01-03-00-000

Related Topics

"Enable/Disable"