DRV.NAME
Description
You can assign a unique name to any drive under the following conditions:
- Only use ASCII characters
- Max length of 10 characters
- No spaces in name
This name is one way to identify the drive in a multiple drive network (for instance, in a TCP/IP network on which multiple drives reside).
From the terminal screen, DRV.NAME returns the name of the drive as ASCII characters.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
No-Name |
Data Type |
String |
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | Yes |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
2031h/0 |
M_01-00-00-000 |