DRV.NVLOAD

Description

DRV.NVLOAD loads all data from the NV memory of the drive into the RAM parameters.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET
Fieldbus Address Attributes Signed?

PROFINET

2788 Command* No
Sercos® III

*For PROFINET, write a value of 0 into the PNU to execute a command.

EtherNet/IP
Instance Data Size Data Type
789 Command None
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

1576

No Command No M_01-06-03-000

Related Topics

DRV.NVLOAD , DRV.NVLIST