DRV.POWERBOARDID
Description
The DRV.POWERBOARDID returns unique identifier for all devices that have power-board with separate power board FPGA.
For all devices that do not have an own power board FPGA, the error message “No power board FPGA exist” will be returned.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
0 to 255 |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-12-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus | Address | Attributes | Signed? |
---|---|---|---|
PROFINET |
2905 | Byte | No |
Sercos® III | 1 Octets |
Instance | Data Size | Data Type |
---|---|---|
906 | 1 Byte | Integer |
Register Address | Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|
1810 |
No | 8 bit | No | M_01-12-00-000 |