DRV.REBOOT

Description

This parameter performs a software reboot when the following command is issued in the WorkBench terminal:

DRV.REBOOT 0xAABBCCDD

WorkBench will disconnect from the AKD when the reboot command is executed. The AKD can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD once rebooted.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-13-08-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

3013 DWord No
Sercos® III 4 Octets
EtherNet/IP
Fieldbus Instance Data Size Data Type
EtherNet/IP 1014 4 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

2842

No 32 bit No M_01-13-08-000