DRV.STOP

Description

This command stops drive motion. In torque and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.

If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.

The following table defines the behavior of DRV.STOP:

Cmdsource Opmode Subopmode Deceleration ramp defined by:
Service Torque - IL.CMD = 0
Velocity - If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used.
Position Service motion If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used.
Motion tasking MT.DEC
Homing HOME.DEC
Fieldbus Torque - Command has no effect.
Velocity
Position
Electronic Gearing Position - GEAR.DECMAX
Analog Torque - Command has no effect.
Velocity
Position

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

35FEh/0

M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2137

Command* No
Sercos® III

*For PROFINET, write a value of 0 into the PNU to execute a command.

EtherNet/IP
Instance Data Size Data Type
138 Command None
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

274

No Command No M_01-03-00-000