DRV.TIME

Description

A continuous time counter in the drive. The timer starts at zero and counts up until it rolls over. If a new value is written to the timer, it continues to count up starting at the written value. The DRV.TIME value is set to zero when the AKD BASIC is powered on.

General Information

Type

R/W

Units

Milliseconds

Range

0 to 4294967295 (~ 49 days)

Default Value

N/A

Data Type

Integer

Start Version

 

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT No
AKD CANopen No
AKD BASIC Yes
AKD SynqNet No
AKD EtherNet/IP No
AKD PROFINET No
AKD Sercos® III No
AKD-N No
AKD-C No

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2529 DWord No
Sercos® III 4 Octets
Modbus
Register Address Is 64 bit? Attributes Signed?

1058

No 32 bit No

Related Topics

DRV.RUNTIME | WHEN.DRV.TIME