ECAT.ENEMCYREQ

Description

This parameter is used to enable or disable the EtherCAT emergency messaging.

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-18-03-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer No
AKD EtherCAT Yes
AKD CANopen No
AKD BASIC No
AKD SynqNet No*
AKD EtherNet/IP No
AKD PROFINET No
AKD Sercos® III No
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.