ECAT.ENEMCYREQ
Description
This parameter is used to enable or disable the EtherCAT emergency messaging.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-18-03-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | Yes |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No* |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | Yes |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.