FBUS.SYNCACQUIREWND

Description

Defines the time window that is used for the starting the synchronization. If the measured (FBUS.SYNCDIST) and target time (FBUS.SYNCDIST) are within this absolute window (for a certain period) the synchronization is successful and FBUS.PLLSTATE will return the locked state.

General Information

Type

NV Parameter

Units

ns

Range

5 to 100,000 ns

Default Value

12,500 ns

Data Type

Integer, U32

Start Version

M_01-14-06-001

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD Profinet Yes
AKD sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see Supported Parameters (➜ p. 1).

Fieldbus

Index/Subindex

Object Start Version

EtherCAT COE and CANopen

5411h/0

M_01-14-06-001

Fieldbus

Address

Attributes Signed?

Profinet

3014

DWord No
sercos® III 4 Octets
Fieldbus Instance Data Size Data Type
EtherNet/IP 1042 4 Byte Integer

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed? Object Start Version

Modbus

2898

No 32 bit No M_01-14-06-001