FBUS.SYNCDIST

Description

This parameter sets time target for synchronization.

General Information

Type

NV Parameter

Units

ns

Range

0 to 2,500,000 ns

Default Value

100,000 ns

Data Type

Integer, U32

See Also

Appendix B: Fieldbus Manuals

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3496h/1 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2180 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
181 4 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

360

No 32 bit No M_01-03-00-000