FBUS.TYPE

Description

FBUS.TYPE shows the active fieldbus type.

0 = Analog

1 = SynqNet

2 = EtherCAT

3 = CANopen

4 = EthernetIP

5 = Profinet

6 = sercos® III

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 6

Default Value

0

Data Type

U8

See Also

Fieldbus Manuals

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2182 Byte No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
183 1 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

364

No 8 bit No M_01-03-00-000