GEAR.SYNCWND
Description
On a drive that is set up as an Electronic Gearing slave, GEAR.SYNCWND can be used to control the drives synchronization status. The slave will be considered synchronized as long as its velocity lies in the range of ±GEAR.SYNCWND around the velocity commanded by the master.
When set to 0, the slave will be synchronized as soon as its velocity is at least the velocity commanded by the master (velocity matching) or always be synchronized (position matching) and will then never change its synchronization state.
General Information
Type |
NV Parameter |
Units |
Depends on UNIT.ACCROTARY or UNIT.ACCLINEAR Rotary: rpm, rps, deg/s, Custom Units/s, rad/s Linear: counts/s, mm/s, µm/s, Custom Units/s |
Range |
Rotary: 0.000 to 15,000.000 rpm 0.000 to 250.000 rps 0.000 to 90,000.000 deg/s 0.000 to 1,250.000 Custom Units/s 0.000 to 1,570.796 rad/s Linear: 0.000 to 1,073,741,824,000.000 counts/s 0.000 to 250.000*MOTOR.PITCH mm/s 0.000 to 250,000.000*MOTOR.PITCH µm/sec 0.000 to 1,250.000 Custom Units/s |
Default Value |
0.000 |
Data Type |
Float |
Start Version |
M_01-14-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | No |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3035 |
DWord | No |
sercos® III | 4 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 1036 | 4 Byte | Velocity |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|---|
Modbus |
2886 |
No | 32 bit | No | M_01-14-06-000 |
Related Topics