HOME.P

Description

This parameter sets the home position. The command and actual position of the drive will be set to this value as soon as a homing event occurs. The homing events differ in each homing mode.

General Information

Type

R/W Parameter

Units

Depends on UNIT.PROTARY or UNIT.PLINEAR

Rotary: counts, rad, deg, Custom Units, 16-bit counts

Linear: counts, mm, µm, Custom Units, 16-bit counts

Range

N/A

Default Value

0

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

607Ch/0

M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2205 DWord Yes
Sercos® III 8 Octets
EtherNet/IP
Instance Data Size Data Type
206 8 Byte Signed Position
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

410

Yes 64 bit Yes M_01-03-00-000

Related Topics

Homing