IP.EOEGATEWAY
Description
IP.EOEGATEWAY displays the EoE gateway IP. If no EtherCat Master with EoE is connected, the return value is 0.0.0.0.
General Information
Type |
RO/Parameter |
Description |
Displays the EoE gateway IP |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type | String |
Start Version |
M_01-18-01-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | Yes |
AKD CANopen | No |
AKD Basic | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD PROFINET | No |
AKD Sercos® III | No |
AKD-N | Yes |
AKD-C | Yes |