JOG.MOVEP
Description
This parameter starts a continuous velocity jog in the positive direction when the drive is in Service Velocity mode or Service Position mode.
The jog moves with velocity JOG.V and accelerate/decelerate using JOG.ACC and JOG.DEC.
General Information
Type |
Command |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
N/A |
Start Version |
M_01-19-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | Yes |
AKD-C | No |