JOG.V
Description
This parameter sets the jog velocity. To activate jog, see JOG.MOVEN and JOG.MOVEP.
General Information
Type |
NV Parameter |
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR |
Range |
0.000 to 15,000.000 |
Default Value |
60.000 rpm |
Data Type |
Float |
Start Version |
M_01-19-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.