MODBUS.CLRERRORS

Description

Clears all errors stored in MODBUS.ERRORS. Error count is set to 0.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-08-03-001

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET No
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Sercos® III
Address Attributes Signed?
2879 Command No
EtherNet/IP
Instance Data Size Data Type
880 Command None
Modbus
Register Address Is 64 bit? Attributes Signed?

1758

No Command No

Related Topics

MODBUS.ERRORS | MODBUS.ERRORMODE