MOTOR.FIELDWEAKENING
Description
Allows a surface permanent magnet motor (MOTOR.TYPE = 0) to operate as an interior permanent magnet motor (MOTOR.TYPE = 6).
This keyword can only be set when MOTOR.TYPE = 0. Any other MOTOR.TYPE will result in an error and MOTOR.FIELDWEAKENING will not be applied.
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-13-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
2983 |
Byte | No |
sercos® III | 2 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 984 | 1 Byte | Integer |
Related Topics