MOTOR.IMID

Description

The value of IL.IMID can be estimated using the motor name plate information.

The following rule should generally be used:

Id root-mean-square approximately equals lr multiplied by the square root of 1 minus open parentheses cos phi close parentheses squared multiplied by 0.8

In which Id is the value for IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).

General Information

Type

R/W

Units

Arms

Range

0 to DRIVE.IPEAK

Default Value

0

Data Type

Float

Start Version

M_01-08-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

5362h /0

M_01-08-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2866 DWord No
Sercos® III 4 Octets
EtherNet/IP
Instance Data Size Data Type
867 4 Byte Float
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

1732

No 32-bit No M_01-08-00-000

Related Topics

Motor View