MOTOR.INFO
Description
MOTOR.INFO returns the production year and week of a Kollmorgen motor. This is supported under following conditions:
- A Kollmorgen motor is used
- The feedback has a manufacture specific memory
- The electronic data sheet of the motor is properly programmed
- The parameter MOTOR.AUTOSET is turned on
If one of the conditions is not true, the parameter returns:
-->MOTOR.INFO
Year: N/A
Week: N/A
If the motor was manufactured in the 36th week in 2015, the parameter returns:
-->MOTOR.INFO
Year: 2015
Week: 36
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
String |
Start Version |
M_01-14-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | No |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Related Topics