MOTOR.NAME

Description

This parameter is used to set the motor name.


  • This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.

General Information

Type

NV Parameter

Units

N/A

Range

20 chars

Default Value

N/A

Data Type

String

See Also

N/A

Start Version

M_01-00-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3899h/0 M_01-19-04-000

Related Topics

Motor View