MOTOR.VOLTMAX
Description
This parameter sets the rated nominal operating voltage for the motor insulation system in Vrms. For instance, if a motor rated for a 480 Vac supply is connected to the drive, then MOTOR.VOLTMAX should be set to 480.
This value also sets the regen resistor and over voltage thresholds in the drive to acceptable values for the motor so that the motor windings are not damaged. Since VOLTMAX is specified as nominal RMS Voltage, the drive will fault if the DC bus VBUS.VALUE exceeds 2x VOLTMAX which provides sufficient margin to be safe and to prevent false trips.
General Information
Type |
NV Parameter |
Units |
Vrms |
Range |
0 to 900 Vrms |
Default Value |
230 Vrms |
Data Type |
Integer |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
EtherCAT COE and CANopen |
3452h/0 |
M_01-00-00-000 |
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
2262 |
Word | No |
sercos® III | 2 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 263 | 2 Byte | Integer |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
524 |
No | 16 bit | No |
M_01-03-00-000 |
Related Topics