MT.LOAD

Description

MT.LOAD reads out a motion task number MT.NUM from the drive. A motion task consists of the following parameters: MT.NUM, MT.P, MT.V, MT.CNTL, MT.ACC, MT.DEC, MT.TNUM, MT.MTNEXT, MT.TNEXT. These parameters belong to the motion task number MT.NUM and are refreshed by MT.LOAD.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

0

Data Type

N/A

See Also

MT.NUM, MT.P, MT.V, MT.CNTL, MT.ACC, MT.DEC, MT.TNUM, MT.MTNEXT, MT.TNEXT, MT.SET

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base No
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC No
AKDSynqNet No
AKDEtherNet/IP Yes
AKDPROFINET Yes
AKDSercos® III Yes
AKD-N Yes
AKD-C No

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2271 Command* No
Sercos® III

*For PROFINET, write a value of 0 into the PNU to execute a command.

EtherNet/IP
Instance Data Size Data Type
272 Command None
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

542

No Command No M_01-03-00-000

Related Topics

Motion Tasks