PL.ERR

Description

PL.ERR reads the position error present when the drive is controlling the position loop. PL.ERR is the difference between the actual position of the motor shaft (PL.FB) and the commanded position of the drive (PL.CMD).  If the drive is not in the position operating mode (DRV.OPMODE = 2), then the PL.ERR value is not generated by the drive and this parameter is read as 0.

AKD BASIC Notes


  • When you enable the position error interrupt (by setting INTR.PL.ERR=1), the Position Error fault is disabled. In situations where it would have occurred, a position error interrupt is generated instead.

General Information

Type

R/O Parameter

Units

counts, rad, deg, (custom units)

Range

N/A  

Default Value

N/A

Data Type

Float

BASIC: Integer

See Also

PL.FB

Start Version

M_01-00-00-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

35C5h/0

Profile Specific SDOs/0

M_01-00-00-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2287 DWord No
Sercos® III 8 Octets
EtherNet/IP
Instance Data Size Data Type
288 8 Byte Position
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

574

Yes 64 bit No M_01-03-00-000

Related Topics

PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop