PL.MOTIONLIMITEN
Description
When PL.MOTIONLIMITEN is set to one, the drive's command velocity will be limited by VL.LIMITP / VL.LIMITN and acceleration and deceleration will be limited by DRV.ACC / DRV.DEC, even when the drive is set to Position Mode.
Since this limitation does not affect position command, it may increase the position error and potentially lead to the drive having a fault due to exceeding the position error limit.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
See Also |
N/A |
Start Version |
M_01-17-05-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
AKD EtherNet/IP | Yes |
AKD PROFINET | Yes |
AKD Sercos® III | Yes |
AKD-N | Yes |
AKD-C | No |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Index/Subindex | Object Start Version |
---|---|
5462h/0 |
M_017-05-000 |
Fieldbus | Address | Attributes | Signed? |
---|---|---|---|
PROFINET |
3122 | Byte | No |
Sercos® III | 2 Octets |
Instance | Data Size | Data Type |
---|---|---|
1123 | 1 Byte | Integer |
Register Address | Is 64 bit? | Attributes | Signed? | Object Start Version |
---|---|---|---|---|
3060 |
No | 8 bit | No | M_01-17-05-000 |
Related Topics