PLS.MODE

Description

PLS.MODE is a bit variable which determines the mode of an individual PLS. Eight PLSs are available in the drive.

Example

Bit Value Behavior

Bit 0 = 0

PLS 1 is monitored continuously.

Bit 0 = 1

PLS 1 is monitored until it is triggered once (single-shot method). The PLS observation can be re-armed using the PLS.RESET command.

Bit 7 = 0

PLS 8 is monitored continuously.

Bit 7 = 1

PLS 8 is monitored until it is triggered once (single-shot method). The PLS observation can be re-armed using the PLS.RESET command.

General Information

Type

R/W Parameter

Units

N/A

Range

0 to 255

Default Value

0

Data Type

Integer

See Also

PLS.EN, PLS.RESET, PLS.STATE, PLS.UNITS, PLS.P1 to PLS.P8, PLS.WIDTH1 to PLS.WIDTH8, PLS.T1 to PLS.T8

Start Version

M_01-02-03-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C No

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

34A3h/3

M_01-02-03-000
PROFINET and Sercos® III
Fieldbus Address Attributes Signed?

PROFINET

2310 Word No
Sercos III 2 Octets
EtherNet/IP
Instance Data Size Data Type
311 2 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

620

No 16 bit No M_01-03-00-000

Related Topics

Programmable Limit Switch