PLS.RESET

Description

This parameter is a bit variable and is used in order to re-arm the corresponding PLS.STATE observation for another single-shot PLS use (see also PLS.MODE).

Example

Bit Value

Behavior

Bit 0 = 0

The PLS 1 observation (PLS.STATE bit 0) is not re-armed.

Bit 0 = 1

The PLS 1 observation (PLS.STATE bit 0) is re-armed.

Bit 7 = 0

The PLS 8 observation (PLS.STATE bit 7) is not re-armed.

Bit 7 = 1

The PLS 8 observation (PLS.STATE bit 7) is re-armed.

General Information

Type

R/O Parameter

Units

N/A

Range

0 to 255

Default Value

N/A

Data Type

Integer

See Also

PLS.EN, PLS.MODE, PLS.STATE, PLS.UNITS, PLS.Px (x=1…8), PLS.WIDTHx (x=1…8), PLS.Tx (x=1…8)

Start Version

M_01-02-03-000
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version

34A3h/2

M_01-02-03-000

PROFINET and Sercos III
Fieldbus Address Attributes Signed?

PROFINET

2327 Word No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
328 2 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

654

No 16 bit No M_01-03-00-000

Related Topics

Programmable Limit Switch