PN.POSSCALE
Description
This parameter sets scaling for PNUs in Profinet which have an index greater than 2000, have the data type float, and are dependent on the position scaling parameters UNIT.PLINEAR or UNIT.PROTARY.
PNU values are scaled by dividing the parameter value by the value of PN.POSSCALE:
PNU value = parameter value (such as PL.FB or HOME.P) / PN.POSSCALE
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
1 to 1,000,000 |
Default Value |
1000 |
Data Type |
Integer |
Start Version |
M_01-13-08-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD PROFINET | Yes |
AKD Sercos® III | No |
AKD-N | No |
AKD-C | No |
Fieldbus Information
Fieldbus | Address | Attributes | Signed? |
---|---|---|---|
PROFINET |
3014 |
DWord | No |