PN.TIMEOUTFTHRESH
Description
Reads the timeout fault threshold for the Profinet Communication Lost Fault (F702). This is the time that is assigned to the drive via the Profinet master. To change the value, set the “watchdog time” or “watchdog factor” through the master. Be advised that setting a high timeout value can lead to the drive not recognizing a lost connection.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-13-11-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | Yes |
AKD sercos® III | No |
AKD-N | No |
AKD-C | No |
Fieldbus Information
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3022 |
DWord | No |
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
2860 |
No | 32 Bit | No |
M_01-13-11-000 |