REC.TRIGMASK

Description

The keyword REC.TRIGMASK is only active when the trigger type (REC.TRIGTYPE) for the recorder is set to 5, which means "Bit Mask Parameter". The trigger is executed once the trigger level (REC.TRGIVAL) matches the data of the trigger parameter (REG.TRIGPARAM) bitwise mask with REC.TIRGMASK.

General Information

Type

Read / Write

Units

N/A

Range

0 to 2^63-1

Default Value

0

Data Type

Integer

See Also

REC.TRIG

REC.TRIGPARAM

REC.TRIGVAL

REC.TRIGSLOPE

REC.TRIGPO

Start Version

M_01-00-00-000

Variants Supported

Variant Supported
AKD Base Yes
AKD with Position Indexer Yes
AKD EtherCAT Yes
AKD CANopen Yes
AKD BASIC Yes
AKD SynqNet Yes*
AKD EtherNet/IP Yes
AKD PROFINET Yes
AKD Sercos® III Yes
AKD-N Yes
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

This keyword is not accessible via fieldbus.