REGEN.REXT

Description

REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.

General Information

Type

NV Parameter

Units

Range

0 to 255

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000
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
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

EtherCAT CoE and CANopen
Index/Subindex Object Start Version
35C2h/0 M_01-00-00-000
PROFINET and Sercos® III
Fieldbus

Address

Attributes Signed?

PROFINET

2369 Word No
Sercos® III 2 Octets
EtherNet/IP
Instance Data Size Data Type
370 2 Byte Integer
Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

738

No 16 bit No M_01-03-00-000

Related Topics

"Regeneration"