REGEN.TESTTO

Description

Regen.TESTTO sets the timeout for the REGEN.TEST command.

General Information

Type Command
Description Sets regen test timeout.
Units ms
Range 1 – 4000 ms
Default Value 1000 ms
Data Type Integer
Start Version M_01-18-06-000
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
AKD-N No
AKD-C Yes

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Fieldbus Information

If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type. For information on SynqNet parameters see SynqNet Supported Parameters.

Related Topics

Regeneration