SD.STATUS

Description

This parameter reads the status of the SD card.

Status Description
0 Ready – an SD card is inserted into the drive and you can read and write to it.
1 Read Only – an SD card is inserted into the drive and the write protection tab on the card prohibits writes.
2 Not Inserted – an SD card is not inserted into the drive.

General Information

Type

R/O

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Start Version

M_01-06-03-000

Variants Supported

Supported by any AKD with an SD Card slot.

Fieldbus Information

Modbus
Register Address Is 64 bit? Attributes Signed? Object Start Version

1688

No 8-bit No M_01-06-03-000

*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.

Related Topics

SD.LOAD | SD.SAVE