SM.DEC
Description
Sets the deceleration ramp for service motion if set to greater than 0.
General Information
Type |
NV Parameter |
Units |
Depends on UNIT.ACCROTARY or UNIT.ACCLINEAR
|
Range |
Note: The range and default values of (custom units)/s² units depend on the values of PIN and POUT. The range and default values listed in this table are derived from the default values of PIN and POUT. Rotary: 0.0 to 833,333.333 rps/s 0.0 to 50,000,000.000 rpm/s 0.0 to 300,000,000.000 deg/s2 0.0 to 4,166,666.752 (custom units)/s2 0.0 to 5,235,987.968 rad/s2 Linear: 0 to 3,579,139,408,000.000 counts/s2 0 to 833,333.333*MOTOR.PITCH mm/s2 0 to 833,333,333.333*MOTOR.PITCH µm/s2 0 to 4,166,666.667 (custom units)/s2 |
Default Value |
0 |
Data Type |
Float |
Start Version |
M_01-13-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet | Yes* |
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
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.
Fieldbus |
Address |
Attributes | Signed? |
---|---|---|---|
Profinet |
3011 |
DWord | No |
sercos® III | 8 Octets |
Fieldbus | Instance | Data Size | Data Type |
---|---|---|---|
EtherNet/IP | 1012 | 8 Byte | Acceleration |
Related Topics