STRING1.DRIVESEOEIPADDRESS to STRING2.DRIVESEOEIPADDRESS
Description
STRINGx.DRIVESEOEIPADDRESS displays the IP address of the Ethernet over EtherCAT interface of all devices connected on string x.
When used without a parameter, it will return a list containing the IP address of all devices on the string.
When used with a parameter, it will display the IP address of a specific device instead, e.g. “STRING1.DRIVESEOEIPADDRESS 3” will display the IP address of the third device on the first string.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
Index: 1 to "number of connected drives" |
Default Value |
N/A |
Data Type |
Index: Integer Value: String |
Start Version |
M_01-18-01-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | No |
AKD-C | Yes |