STRINGx.DRIVESIPADDRESS
Description
STRINGx.DRIVESIPADDRESS displays the IP addresses of all devices connected on string x.
When used without an index number it will return a list containing the IP addresses of all devices on the string.
When used with an index number it will display the IP address of a specific device instead, e.g. STRING1.DRIVESIPADDRESS 3 //displays the IP address of the 3rd device on the first string.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
N/A |
Data Type |
String |
Start Version |
M_01-16-02-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD PROFINET | No |
AKD Sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
The -C Central Power Supply (➜ p. 1) | STRINGx.NODECOUNT