STRINGx.DRIVESISFAULTED
Description
STRINGx.DRIVESISFAULTED displays the fault status of the drives connected to the AKD-C on string x. Each bit represents the fault status of one drive, starting with the fault status of the first drive in the least significant bit.
- 0 – drive has no faults
- 1 – drive has faults
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
0 to 255 |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-17-01-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD PROFINET | No |
AKD Sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
The AKD-C Central Power Supply