STRINGS.FORCEDOWNLOAD
Description
This keyword will power cycle all AKD-Ns connected to the AKD-C and boot them up in "firmware download" mode (when keyword is set to 1) or in operational mode (when keyword is set to 0). This allows AKD-N drives to be recovered when their operational firmware has been corrupted. Note that the Bus power cannot be applied to the AKD-C/Ns when this keyword is issued since the logic power to the AKD-N drives will be turned off and back on. A fault will be generated if the Bus power is applied and this keyword is issued.
Value | Description |
---|---|
0 | Power cycles the AKD-Ns and boots them up in operational mode for normal operation |
1 | Power cycles the AKD-Ns and boots them up in “firmware download” mode. |
General Information
Type |
R/W Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Boolean |
Start Version |
M_01-14-00-003 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD Profinet | No |
AKD sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics